Hand saws are versatile tools that come in many varieties, each designed for specific cutting tasks. While some hand saws are intended for general use, others are precision-engineered for specialised applications. Understanding these differences is essential for selecting the right tool for your project.
It's important to note that the terminology used for hand saws can vary among suppliers, manufacturers, and users, leading to potential confusion. For instance, you might encounter various names for similar saw types when shopping for a timber saw, including:
- Ripping Saw: Designed for cutting wood along the grain. Typically, 24 to 26 inches long with 4 to 7 TPI (teeth per inch), it cuts aggressively but leaves a rough edge.
- Crosscut Saw: Used for cutting across the grain of wood. Usually measuring 24 to 26 inches long with 8 to 11 TPI, it produces smoother cuts compared to ripping saws.
- Panel Saw (Shortcut or Box Saw): Shorter than standard crosscut saws, panel saws are portable and ideal for making crosscuts in larger sheets of wood, such as plywood or MDF.
- Short Cut Saw: A compact version of a panel saw designed for quick cuts in various materials.
- Wood Saw: A general term that can refer to any hand saw used primarily for cutting wood.
- Tenon Saw: This type of back saw is used for making precise cuts in wood joints and typically features a high TPI for clean edges.
- Back Saw: Known for its rigid back that prevents kinking, this saw is perfect for making precise cuts in molding and trim work.
- Dovetail Saw: Similar to a back saw but smaller with finer teeth; it is ideal for making intricate cuts necessary for dovetail joints.
- Pruning Saw: Designed specifically for cutting branches and shrubs in gardening tasks; it often features curved blades for better manoeuvrability.
- Plasterboard Saw: Also known as a drywall saw, this tool is designed to cut through wallboard and gypsum quickly and efficiently.
- Coping Saw: Featuring a thin blade held in a deep frame, the coping saw is perfect for intricate cuts such as coping joints in moldings. It can also cut through plastic and light metals.
- Fine Finish Saw: This type of saw is designed for achieving smooth finishes on wood surfaces.
- Fretsaw: Similar to the coping saw but with a finer blade, it is used for detailed work and intricate designs.
- Hacksaw: Primarily used for cutting metal, hacksaws feature fine teeth held under tension in a steel frame. They are versatile enough to cut through various materials, including plastic.
- Frame Saw: A traditional hand saw with a frame that allows the use of different blades depending on the task at hand.
- Bow Saw: Designed primarily for outdoor use, bow saws excel at cutting tree branches and logs quickly.
- Hardpoint Saw: These basic saws feature induction-hardened teeth and plastic moulded handles. They are ideal for general-purpose cutting but cannot be resharpened once dull.
- Keyhole Saw: A thin blade designed specifically for cutting small circles and curves in wood or drywall.
- Punch Saw: Used mainly in woodworking to create holes or cut curves in various materials.
- Compass Saw: Longer than a keyhole saw; it is used for heavier tasks like cutting holes in subflooring or creating larger curves.
- Pull Saw: Cuts on the pull stroke, providing greater control and reducing the chance of kinking during use. This design is particularly useful in fine woodworking applications.
- Dozuki Saw: A Japanese-style pull saw that features a fine blade ideal for precise cuts in woodwork.
- Ryoba Saw: Another Japanese hand saw with two different tooth patterns on each side of the blade, one side is designed for ripping while the other is meant for crosscutting.
- Kataba Saw: A single-edged Japanese saw that excels at making clean cuts across the grain of wood.
- Pole Saw: Designed with an extended reach, pole saws are used primarily for pruning high branches without needing a ladder.
- Veneer Saw: A specialised tool used to cut thin sheets of veneer without tearing or damaging the material.
The overlap in terminology often results in several names being used interchangeably, even when referring to what appears to be the same basic type of hand saw. In many cases, the distinctions between these subtypes can be subtle. For example, wood saws designed for straightforward timber cutting may be labeled as rip saws, panel saws, or crosscut saws depending on their intended use.
Similarly, tenon saws might be categorised as back saws or dovetail saws by different suppliers. Various hand saws designed for making holes or curves, such as punch saws, keyhole saws, compass saws, and fretsaws, may also serve similar purposes despite their unique designs.
To simplify understanding, this guide will focus on four major categories of hand saws based on their primary material uses: wood saws, metal saws, plasterboard saws, and pruning saws.