Recently searched
      • Published 15 May 2024
      • Last Modified 14 Jun 2024
    • 11 min

    Understanding Network Switches: A Complete User Guide

    Find out more about how network switches are used, how they work, and what types are available in our guide.

    Network switches are vital components in any wired network setup. This guide delves into the essentials of network switches, explaining their role, functionality, and the variety of models on the market. From basic unmanaged switches to advanced managed models, we'll help you understand which type best suits your needs and how to maximise your network's efficiency.

    What is a Network Switch?

    A network switch is a wired hub device primarily used to connect multiple users and devices to a single computer network. In home, business, or industrial computer networking and connectivity setups, the primary function of network switches is to create a physical link between online resources and devices through a single multi-port access point. This setup allows users on the same network to share access to various resources and devices.

    Typical examples of resources connected via network switches include:

    • Incoming internet connections, usually facilitated by a router.
    • Various external storage and file-sharing devices, such as high-capacity hard drives or server arrays
    • An assortment of key hardware and peripherals, including desktop computers, laptops, gaming consoles, smart TVs, UPS power supplies, and printers.

    Network switches are often called ethernet switches or LAN switches (Local Area Network). These terms highlight their reliance on cabled connections to facilitate networking activities within a relatively confined physical area, such as a single office.

    How Does a Network Switch Work?

    To fully understand how an ethernet switch operates, it’s essential to be aware of the different types available. While we’ll explore these in detail later, let’s first address the fundamental question: 'What does a network switch do?'

    A network switch serves as a central hub in a computer network, providing wired connections for multiple devices and resources. This allows data, internet connectivity, and other resources to be shared among the network users. Some switches also feature an onboard software interface that lets you manage and control these connections.

    At its simplest, a network switch can be considered as a large USB hub, but one specifically made to accept ethernet or RJ45 cables. This enables multiple devices to share a single wired internet or data connection.

    A standard internet router will likely include at least one built-in ethernet port, but probably not more than two or three for midrange models. To provide a far more robust connectivity solution that allows you to hook in multiple devices and resources - thus creating a more complex Local Area Network, or LAN – you will need to add a network switch.

    Network switches are usually connected directly to a router or server. Their primary function is to offer more ports for plugging in additional ethernet cables, thereby expanding the network. The type and model of LAN switch you choose will largely depend on the size and scope of the network you intend to create.

    Accordingly, the number of ethernet ports a given switch provides can range from as few as three, up to 50 and beyond. Where heavy-duty industrial network switches are needed, it’s even possible to find versions offering 100 or more, although these are considerably less common.

    What are the Different Types of Network Switches?

    Network switches come in various types, each tailored for specific applications. The main types of network switches include:

    Stackable Network Switch

    A stackable switch can function as a standalone unit or be connected with multiple other stackable switches to expand connectivity. When combined, these switches operate as a single, larger switch with a combined port count, providing enhanced connectivity and performance.

    Unmanaged Network Switch

    This is the simplest type of switch, ideal for quickly adding more ethernet ports to your network. Unmanaged switches require no configuration or input from the user beyond connecting devices with ethernet cables, and as such are often referred to as ‘plug and play’ or a simple LAN switch. They are commonly used in small offices or commercial settings where advanced network management is not required.

    Managed Network Switch

    These switches are used for greater control and advanced functionality. Managed network switches offer a built-in dashboard or similar interface, often displayed through a connected web browser. This provides admin-level users with a suite of tools for monitoring and tweaking various aspects of the network configuration as traffic flows through it.

    Depending on the model in question, options might include anything from access privileges, port mirroring and redundancy, to data transfer rates (port speed), device prioritisation and more. Managed network switches can either be designed as a fully manual switch or a smart switch. The former tends to be the most versatile and is ideal for complex networking requirements (server and enterprise-level setups), while smart switches are usually more user-friendly but provide a limited range of configuration options.

    PoE Network Switch

    Regardless of whether you opt for a managed or unmanaged networking hub, you may also choose a PoE or ‘Power over Ethernet’ switch.

    These models enable power to be transferred to compatible devices via connected RJ45 cables, as opposed to just data. If your network includes several PoE-enabled devices, choosing a switch with this feature included can result in a far neater and more flexible solution, dramatically cutting down on excess cabling (notably to wall sockets), and enhancing overall LAN scalability and reliability.

    Please note that not all hardware is intrinsically PoE compatible – you will need to check the specifications for each device you wish to connect.

    Understanding the Difference Between Network Switches and Routers

    Many people often confuse network switches and router due to their closely related functions. However, the key difference between these two pieces of hardware is fairly straightforward once you grasp their distinct roles.

    A network switch allows multiple devices within the same network to communicate with each other. It acts as an intermediary, ensuring that data packets are efficiently sent to the correct device within the local network.

    On the other hand, a router connects multiple different networks, enabling them to communicate with one another. For example, a typical ISP-supplied Wi-Fi router facilitates communication between the external internet and the local network within your home or office. Unlike a router, a network switch cannot connect to external networks; its purpose is to enhance the internal network's flexibility and performance that the router connects to the internet.

    The confusion between routers, switches, and hubs often arises because some devices integrate features from all three types of hardware, typically by including multiple built-in ethernet ports. Despite these overlapping features, it is important to understand that the fundamental functions of a router, hub, and switch remain distinct, even when combined into a single device.

    What Speeds Can Network Switches Handle?

    When choosing the ideal ethernet switch for your networking needs, suppliers and manufacturers usually categorize their products by speed. The primary speed categories are:

    • Fast Ethernet switches (FS) - 10/100 Mbps (standard IEEE 802.3u)
    • Gigabit network switches (GS or JGS) - 10/100/1000 Mbps (standard IEEE 802.3-2008)
    • Ten-gigabit network switches (GSS) - 10/100/1000/10000 Mbps (standard IEEE 802.3a)

    Additionally, you might come across other ethernet speeds and standards, such as 2.5 Gbps, 5 Gbps, 25 Gbps, 40 Gbps, 50 Gbps, or even 100 Gbps, which are typically designed for specialised applications.

    It's important to remember that the most suitable network switch for home use might not be the best choice for small businesses, industrial settings, or enterprise environments.

    In fact, each of these applications will have considerably different requirements to consider, largely depending on the scale and speed of connectivity you need to create a stable and strong-performing network. While speed is always an important consideration, another key specification is the number of ports the specific switch offers.

    More ports mean greater flexibility across the network, but the amount of traffic able to flow through the network at any one time - in other words, the number of connected devices and users a network can comfortably support - will be limited by various factors, not least the bandwidth of your internet connection.

    How Many Network Switch Ports Do You Need for Your Network?

    In trying to decide how many network switch ports a particular setup requires for optimal convenience and performance, it’s wise to consider the following factors:

    • How many wired devices you want to connect, bearing in mind potential future device purchases
    • How much you are willing to spend on a network switch
    • Whether you would prefer to use a managed or unmanaged switch
    • Whether you require or can make use of advanced PoE models (either now or in the future)
    • What sort of bandwidth your current router and/or internet connection can comfortably support, and whether you may need to upgrade

    Popular choices for home networking often include small-to-medium sized hubs, such as 4-port5-port or 8-port network switches. Meanwhile, while more complex enterprise or server networks may require far more capable hardware such as a 64-port PoE switch.

    Popular Network Switch Brands

    Some of the most popular brands known for the quality, reliability, and advanced functionality of their network switches and related products include:

    FAQs

    Related links